The procedures below cover the basic functionality of the LS PLC, and cover most tasks you need to complete to get up and running.
Building and powering the LS PLC rack
Getting Connected out of the box (USB and Ethernet comm)
Using the Reset PLC, Clear PLC, and Clear All PLC Commands
Creating Base PLC variables & Variable Export and Import
Analog Module Setup
Digital IO Module setup
Monitoring IO and Tags
Finding and Cross Referencing Used Devices and Tags
Online Editing in XG5000
PID Function Example
Comparing Two Projects in XG5000
Renaming a Variable in XG5000
Forcing I/O with XG5000
Updating Module OS
Pulse Catch Functionality