AutomationDirect adds PID control functionality to CLICK Ethernet PLCs
![]()
Cumming, GA --- September 18, 2019 ... PID loop control capability (up to 8 loops simultaneously) has been added to the CLICK® Series of stackable, Ethernet-capable micro brick PLCs.
CLICK PID control is streamlined with only the features that most users need, including direct or reverse acting control, pulse width modulated control outputs, bumpless transfer, anti-windup, auto-tuning, process variable alarms, process variable limits, control output limits and error deadband.
The CLICK PID monitor gives access to and charts all PID parameters needed to test and tune the PID loops. An auto-tune interface sets up and initiates the auto-tuning feature.
CLICK PID control is simple. With the ability to configure up to 8 PID control loops updating at 100ms, CLICK provides the most affordable PID available, starting at only $183.00 for a standalone CLICK Ethernet analog PLC.
Learn more by visiting www.automationdirect.com/CLICK-PLC
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact:
Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
High resolution image: 300 dpi TIF (right click and Save Target As ...)