StrideLinx Cloud Notify License for remote alarms and messages from AutomationDirect
![]()
Cumming, GA --- September 6, 2018 ... The new StrideLinx Cloud Notify License is an add-on service that provides remote "alarm" emails and push notifications when control limits are exceeded on HMI / PLC devices connected to the StrideLinx VPN router.
The service provides customized alarm names, priority level and instructions for each alarm, and customized alarm recipients. Cloud Notify expands StrideLinx data services by allowing customers to receive remote notification when a process variable in their plant or machine is out of spec.
StrideLinx provides secure, reliable access over the "industrial internet" to field devices for the remote visibility needed in today's connected world. Cloud connect any Ethernet-ready devices at a reasonable, low cost. Connect to multiple site locations all from one browser to monitor or troubleshoot multiple systems without requiring an on-site visit.
The StrideLinx Cloud Notify license from AutomationDirect is a one-time $210.00 purchase; a free 30-day trial is available.
To learn more, visit www.automationdirect.com/stride-linx
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact:
Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
High resolution image: 300 dpi TIF (right click and Save Target As ...)