AutomationDirect adds BRX Analog I/O Expansion Modules
![]()
Cumming, GA --- September 20, 2017 ... The versatile BRX PLC system from AutomationDirect combines powerful features in a compact, stand-alone footprint. One of the unique features of the BRX platform is its ability to expand its capability to fit the application. New analog I/O expansion modules are available in high-resolution current/voltage and temperature models.
Starting at $187.00, two 8-channel analog current and voltage input modules and two 8-channel current and voltage output modules are available. Current signal ranges are 0-20 mA, 4-20 mA; voltage ranges are 0-5 VDC, 0-10 VDC, +/- 5 VDC, +/- 10 VDC. Input and output signal resolution is 16-bits (external 24 VDC required).
The new 4-channel temperature module, priced at $194.00, supports type J, E, K, R, S, T, B, N, C thermocouples. The module can also be configured for 4-channel millivolt level analog inputs.
These analog expansion modules give the user the ability to add analog I/O as needed for process control applications. Each is clearly identified by the module's front panel color scheme and symbol. Expansion modules easily snap onto the side of any BRX Micro PLC Unit (MPU) creating a rugged PLC platform. Once the expansion module has been snapped in place, the software automatically discovers the I/O with little to no additional setup required. Do-more! Designer programming software for the BRX PLC is a free download with no key code required.
BRX PLC hardware is engineered, manufactured and supported in the U.S. by industrial automation veterans. With hardware design and fabrication facilities located in Tennessee and Florida, the BRX PLC platform delivers high quality at a very attractive price.
Learn more by visiting: www.automationdirect.com/brx-plcs
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact:
Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
High resolution image: 300 dpi TIF (right click and Save Target As ...)