AutomationDirect Adds More Touch Panels to the C-more HMI Line
![]()
Cumming, GA --- November 15, 2017 ... AutomationDirect's C-more EA9 series of touch screen HMIs now includes a 10-inch widescreen model and a 15-inch base model touch panel.
The new C-more 10-inch full featured EA9-T10WCL widescreen color TFT touch panel ($685) has three serial ports, an Ethernet 10/100BaseT port, two USB 2.0 ports, one slot for SD memory card and audio line out. Widescreen resolution is 1024 x 600 pixel WSVGA in 64k colors.
The C-more 15-inch base model EA9-T15CL-R color TFT touch panel is $1299.00 and includes one Ethernet 10/100BaseT port, one serial port, two USB ports and two SD memory card slots. Screen resolution is 1024 x 768 pixel XGA in 64k colors.
Both touch panels are 12-24 VDC powered and an optional attachable AC power adapter is available. The panels are NEMA 4/4X and IP65 rated (for indoor use only) and are programmed using the EA9-PGMSW programming software, priced at $99.
C-more HMI touch panels have UL, cUL & CE agency approvals and are backed by a 2-year warranty.
To learn more, visit: www.automationdirect.com/c-more
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact:
Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
High resolution image: 300 dpi TIF (right click and Save Target As ...)