DYMO XTL Series Industrial Label Printers from AutomationDirect
![]()
Cumming, GA --- March 27, 2019 ... XTL series label makers simplify industrial labeling with a large, viewable screen, intuitive controls, and a wide range of functions. XTL series label makers can print using continuous tape, pre-sized labels, heat-shrink tubes, and small format safety labels.
The XTL 300 is a smaller, lighter system ideal for on-the-go label making, capable of printing up to 1 inch (24mm) wide labels. The XTL 500 has a touch screen, more features, and the ability to print up to 2-1/8 inch (54mm) wide labels.
XTL labels come as all-in-one cartridges with the labels and printing tape rolled up inside or as laser compatible printer sheets. Label types include heat-shrink tubing labels, wire/cable wrap labels, pre-sized safety / RTK (right-to-know) labels, permanent flat surface labels, all-purpose vinyl labels and self-laminating laser printer label sheets.
Starting at $209.00, DYMO label maker printers have a 3-year warranty and include a rechargeable battery, charger and USB cable.
To learn more, visit www.automationdirect.com/label-makers
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact:
Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
High resolution image: 300 dpi TIF (right click and Save Target As ...)