Complete Stratus Vortex Cooler Kits from AutomationDirect
![]()
Cumming, GA --- March 14, 2018 ...
AutomationDirect has added complete vortex cooler assemblies to its enclosure thermal management lineup. New Stratus® vortex cooler kits include everything needed to implement enclosure cooling. The kits include Stratus vortex cooler with distribution tube and muffler, a Stego adjustable thermostat, a NITRA pneumatic filter/regulator with NITRA 5-micron filter element and a NITRA 2-way 2-position solenoid valve. Stratus vortex cooler kits are priced at $349.00.
Stratus vortex coolers have cooling capacities from 500 to 2,500 BTUH; vortex cooler advantages include small physical size, cools without refrigerants (no CFCs, HCFCs), exceptionally reliable with no moving parts and vortex coolers are suitable for harsh environments.
The all stainless steel Stratus vortex cooler mounts in a single 3/4" electrical conduit knockout, and relief valves and seals are built-in which enable the units to maintain the sealed nature of NEMA 4, NEMA 4X and NEMA 12 enclosures.
To learn more, visit www.automationdirect.com/enclosure-vortex-coolers
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact:
Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
High resolution image: 300 dpi TIF (right click and Save Target As ...)