More BRX PLC I/O Expansion Modules from AutomationDirect
![]()
Cumming, GA --- June 6, 2018 ... AutomationDirect has added more I/O expansion modules to its BRX Micro PLC product line. BRX I/O expansion modules add digital and analog I/O as needed to expand machine and process control applications. BRX expansion modules easily snap onto the side of any BRX Micro PLC Unit (MPU) or the new BRX Remote I/O controller.
Three new 32-point discrete I/O and five analog I/O expansion modules as well as three new temperature input modules have been added. Three 4-channel analog input and two 4-channel analog output modules are now available with current and voltage signal options.
Current signal ranges are 0-20 mA, 4-20 mA; voltage ranges are 0-5 VDC, 0-10 VDC, +/- 5 VDC, +/- 10 VDC. Max input and output signal resolution is 16-bits.
Also added are 8-channel Thermocouple input, 6-channel RTD input and 8-channel Thermistor input modules; all with 16-bit resolution.
Backed by a 2-year warranty, the new 32-point BRX discrete I/O modules are $99.00, and the analog I/O expansion modules start at $134.00.
To learn more, visit www.automationdirect.com/brx-plcs
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact:
Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
High resolution image: 300 dpi TIF (right click and Save Target As ...)