View more from 6" C-more Micro-Graphic Panels
![]()
Cumming, GA --- July 2, 2008 --- AutomationDirect's C-more Micro-Graphic panel line now includes six-inch display models. The new touch style graphic/text panels offer a 320x240 pixel graphical display that supports bitmap files. Used in a horizontal orientation, the 6-inch C-more micro supports 40 lines by 80 characters of static text; 53 lines by 60 characters are supported in vertical orientation. Two optional keypad bezels are available for either horizontal or vertical panel mounting.
. C-more 6" micro-graphic panels are equipped with drivers to support all DirectLOGIC protocols as well as Allen-Bradley DF1 Full duplex, Allen-Bradley DF1 Half duplex, Allen-Bradley PLC5 DF1, AB DH485, Omron Host Link, Omron FINS serial, GE SNPX, Mitsubishi Melsec FX, Siemens PPI, and Entivity Modbus RTU. The C-more 6" panels are priced at $299. The free panel configuration software features a built-in project simulator. The latest software can be downloaded at http://C-MoreMicro.AutomationDirect.com
AutomationDirect sells over 6,500 feature-packed products through its Online Automation Superstore and 2,000-page catalog. The company offers its customers high-quality automation products at prices well below the industry average, 24-hour order entry with same-day shipping on in-stock items, the best documentation in the industry, and award-winning sales and technical support For a free catalog, access their Web site at www.automationdirect.com or call 800-633-0405.
Editorial Contact:
TJ Johns
Phone: 678-455-1730
Email: tjohns@automationdirect.com
Download high resolution image: 300 dpi TIFF