ProductivityOpen Arduino-compatible Controller from AutomationDirect
![]()
Cumming, GA --- January 29, 2019 ... The open-source Productivity®Open platform provides all the great features of a standard Arduino plus the added power and reliability of an industrial controller. The processor circuit of the P1AM-100 Arduino-compatible CPU is designed to mimic the Arduino MKRZero microcontroller. The P1AM-100 is compatible with most available Arduino MKR format shields, and/or the industrially-hardened ProductivityOpen shields, and can utilize most Arduino sketch programs found on open-source websites.
Using the readily-available Arduino integrated development environment (IDE), the P1AM-100 is programmed using C++ code; the ProductivityBlocks graphical programming interface uses a more visual approach that simplifies coding and reduces syntax errors.
The P1AM-100 CPU supports the full suite of Productivity1000 I/O expansion modules, including: discrete, analog, temperature, relay, high-speed input, pulse-width-modulation. The industrial-grade P1AM-100 Arduino-compatible CPU is $49.00.
Priced from $32.00, available ProductivityOpen UL-certified shields include the P1AM-ETH Ethernet shield and the P1AM-GPIO general purpose I/O shield. The P1AM-PROTO shield is also available for creating customized shields in the MKR form factor.
The Arduino-compatible ProductivityOpen Controller from AutomationDirect is cULus listed, CE approved and backed by a two-year warranty.Learn more by visiting www.automationdirect.com/arduino-cpu
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact:
Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
High resolution image: 300 dpi TIF (right click and Save Target As ...)