Wider range of ProSense™ Pressure Sensors now available from AutomationDirect
![]()
Cumming, GA --- January 14, 2009 --- AutomationDirect has extended the ProSense line of pressure sensors and switches to widen the sensing ranges available. The series now includes pressure switches with adjustable setpoints from 0 to 5,800 psi, as well as transmitters in ranges from 0-15 to 0-3000 psi with output options of 4 to 20mA or 0 to 10 Volts. Transmitters with a measuring range of 0 to 100 inches of water column have also been added. ProSense pressure sensors start at $89. To see the complete ProSense line, visit www.automationdirect.com.
AutomationDirect sells over 7,000 feature-packed products through its Online Automation Superstore and 2,000+ page catalog. The company offers its customers high-quality automation products at prices well below the industry average, 24-hour order entry with same-day shipping on in-stock items, the best documentation in the industry, and award-winning sales and technical support For a free catalog, access their Web site at www.automationdirect.com or call 800-633-0405.
Editorial Contact:
TJ Johns
Phone: 678-455-1730
Email: tjohns@automationdirect.com
Download high resolution image: 300 dpi TIFF