STRIDE Industrial MQTT Gateways from AutomationDirect
![]()
Cumming, GA --- August 7, 2019 ... The STRIDE® MQTT gateway connects industrial Modbus devices to an MQTT cloud-based data logging solution. MQTT (Message Queuing Telemetry Transport) is a machine-to-machine "Internet of Things" connectivity protocol that provides low power usage, minimized data packets, and efficient distribution of information to one or many receivers.
The STRIDE MQTT gateway provides easy hardware setup to add Modbus RTU/TCP devices to an existing MQTT cloud data collection platform. The MQTT gateway interfaces with up to 32 Modbus devices; wired and Wi-Fi gateway models are available.
The STRIDE MQTT Gateway is the hardware component only of an MQTT cloud-based data logging solution. The user must have an existing cloud computing service account from a cloud services provider.
Starting at $215.00, STRIDE MQTT Gateways from AutomationDirect are CE marked, FCC tested and have a one-year warranty.
Learn more by visiting www.automationdirect.com/mqtt-gateways
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact:
Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
High resolution image: 300 dpi TIF (right click and Save Target As ...)