Continuous Flexing Cut-to-Length Motor Supply Cables from AutomationDirect
![]()
Cumming, GA --- August 22, 2018 ... Continuous flexing motor supply cable is now available from AutomationDirect in customer specified one-foot increment lengths. igus Chainflex® continuous flexing CF30 and CF31 motor supply cables are specifically designed, tested, and manufactured to be exposed to constant flexing, providing a cable service life between 5 million and 10 million cycles.
The cables are available with four unshielded (CF30 series) or four shielded (CF31 series) conductors in 16 AWG to 2 AWG sizes. Individual conductors are bare copper and stranded for flexing applications. Conductor insulation is a black TPE mixture that is sunlight and oil resistant and flame retardant. Chainflex cables have a unique jacket tear strip that allows the outer jacket to be easily stripped back from the conductors to the desired length.
Starting at $1.41 per foot, the cables are cut to length in one-foot increments with a 10 or 20-foot minimum depending on cable gauge. The price per foot is the same per cable AWG regardless of length ordered.
Cut-to-length cable eliminates waste and lowers cost (only as much cable as required is purchased). There are no cut charges (and no shipping charges on orders over $49). Cable is cut to length at AutomationDirect's own UL Certified respooling facility and is available for same day shipping if ordered by 6:00pm ET.
To learn more, visit www.automationdirect.com/motor-supply-cable
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact:
Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
High resolution image: 300 dpi TIF (right click and Save Target As ...)