More Compact Limit Switch Connection Options from AutomationDirect
![]()
Cumming, GA --- April 5, 2017 ... AutomationDirect has expanded its AEM2G series compact limit switch line to include more electrical connection options. Four electrical connection types are now available for the AEM2G series of compact limit switches. 5-Pin M12 Quick Disconnect (bottom and right exit) and 3m pre-wired pigtail cable (right exit) connection options have been added to the existing 3m pre-wired pigtail cable (bottom exit) connection. The choice of connection types provides more convenient limit switch installation options.
AEM2G series compact limit switches have die cast metal housings that are epoxy resin filled for IP67 rating and are equipped with one normally-open and one normally-closed contact. These compact limit switches have standard U.S. 25mm mounting hole spacing and are available in a variety of actuator types including metal plunger, lever, rod actuator, and spring actuator. Contact types include both snap-action and slow-make/slow-break.
AEM2G series compact limit switches start at $21.00, have a 1-year warranty and are UL and CE approved.
For more information, visit: www.automationdirect.com/limit-switches
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact:
Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
High resolution image: 300 dpi TIF (right click and Save Target As ...)