|
D2-DCM and D3-DCM Update
Process
STEP 1: Configure DCM
for update mode
- Remove jumper JP1
- Select the secondary address
(1-90)
- Select the baudrate and
parity
- Put DCM into the Base
- Connect the communication
cable (D3-DSCBL-2) between your computer and the DCM
- Power-Up the base
- Check the LED pattern
UPDATE mode -> LED ON: PW,OK,EQ,HD
PW[*] [*]OK
NK[ ] [*]EQ
TO[ ] [*]HD
MA[ ] [ ]DT
Internal RAM error -> LED BLINK: TO,DT
PW[ ] [ ]OK
NK[ ] [ ]EQ
TO[+] [ ]HD
MA[ ] [+]DT
STEP 2: Start the update
tool
- Start Module Update Tool
- Select Comm. Port, baud
rate and parity
- Select data file
- Set secondary address.
STEP 3: Start the update
- Click [Start] button.
Starting DATA send.
DCM LED pattern
data recieve -> LED ON: HD
PW[*] [ ]OK
NK[ ] [ ]EQ
TO[ ] [+]HD
MA[ ] [ ]DT
data send -> LED ON: DT
PW[*] [ ]OK
NK[ ] [ ]EQ
TO[ ] [ ]HD
MA[ ] [+]DT
Broadcast Mode
data recieve -> LED ON: EQ
PW[*] [ ]OK
NK[ ] [+]EQ
TO[ ] [ ]HD
MA[ ] [ ]DT
- [Write OK] message appears
when the operation is complete
- If you click [Cancel] button,
operation is terminated
STEP 4: Confirm update
Check LED pattern
Write or Verify OK = LED ON: PW,OK,EQ,HD,DT,MA
PW[*] [*]OK
NK[ ] [*]EQ
TO[ ] [*]HD
MA[*] [*]DT
Write Error = LED ON: PW,OK,NK,HD,DT
PW[*] [*]OK
NK[*] [ ]EQ
TO[ ] [*]HD
MA[ ] [*]DT
Verify Error = LED ON: PW,OK,NK,EQ,DT
PW[*] [*]OK
NK[*] [*]EQ
TO[ ] [ ]HD
MA[ ] [*]DT
STEP 5: Configuring the
DCM for normal run mode
- Power-OFF system
- Remove DCM from the base
and install jumper JP1
- Place the module into base
and apply power again
- If NK,TO,MA,EQ,HD,and DT
LEDs blink, the update operation was not successful, and you should return to
Step 1
PW[+] [ ]OK
NK[+] [+]EQ
TO[+] [+]HD
MA[+] [+]DT
|
|